Safety Partner OK Indicator
The safety partner has an OK status indicator.
State | Description |
|---|---|
Off | No power is applied. |
Green | The safety partner is operating with no faults. |
Red | One of the following is true:
|
Flashing red | The controller is configured for SIL 2 operation, but a safety partner is installed. |
Provide Feedback