Preface
This manual provides information to help you design a system, operate a
ControlLogix®
or GuardLogix®
-based controller system, and develop applications. You must be trained and experienced in the creation, operation, and maintenance of safety systems.
For information on Safety Integrity Level (SIL) and Performance Level (PL) requirements and safety application requirements, see the GuardLogix 5580 and Compact GuardLogix 5380 Safety Reference Manual, publication 1756-RM012.
The procedures in this manual use the
Studio 5000 Logix Designer®
application. For information about using FactoryTalk® Design Studio™
software, see the FactoryTalk Design Studio Quick Start, publication FTDS-QS001.Provide Feedback