Universal Remote I/O (RIO) Communication
For communication in a Universal RIO network, you have three module options for use in the
ControlLogix®
chassis. This table lists the RIO modules and capabilities.Module | Description |
|---|---|
1756-RIO, 1756-RIOK |
|
1756-DHRIO, 1756-DHRIOK |
|
756-DHRIOXT |
|
When a channel on the 1756-DHRIO or 1756-DHRIOXT module is configured for Universal RIO communication, the module acts as a scanner for the network. The controller communicates to the module to send and receive the I/O data on the Universal RIO network.
The 1756-RIO module can act as a scanner or adapter on a Universal RIO network. The 1756-RIO module transfers digital, block transfer, analog, and specialty data without message instructions.
Universal RIO Network
Communicate Over a Universal RIO Network
As you design your Universal RIO network, remember the following:
- All devices that are connected to a Universal RIO network must communicate with the same communication rate. Available rates include the following:
- 57.6 Kbps
- 115.2 Kbps
- 230.4 Kbps
- You must assign unique partial and full racks to each channel used in Remote I/O Scanner mode. Both channels of a 1756-DHRIO or 1756-DHRIOXT module cannot scan the same partial or full rack address. Both module channels can communicate to 00…37 octal or 40…77 octal, but each channel can communicate only with one address at a time in whichever of these two ranges it falls.
Provide Feedback