DeviceNet Communication Devices
This table lists the available
DeviceNet®
bridge and linking devices that can be used with the DeviceNet®
network.Module | System | Description |
|---|---|---|
1756-DNB, 1756-DNBK | ControlLogix® GuardLogix® |
|
1788-EN2DNR | ControlLogix® | Links an EtherNet/IP™ network to a DeviceNet® network. |
1788-CN2DN | ControlLogix® | Links a ControlNet® network to a DeviceNet® network. |
A ControlLogix controller requires two connections for each 1756-DNB module:
- One connection for module status and configuration
- One rack-optimized connection for device data
Provide Feedback