Popup
A popup is a small window that appears superimposed on the screen. It opens in response to a triggered action. An event configured with a
Popup Open
command opens a popup. If the event is a touch press event on a button, selecting the button opens the popup. A state change to a graphic element, such as the graphic element changing colors, can open a popup automatically. To verify which action opens a popup, contact the HMI designer.Only one popup can open at a time. If the contents of the popup is larger than the popup, the contents appear clipped at the edges of the popup. It is not possible to view clipped content.
Touching elsewhere on the screen or selecting
on the caption of the popup closes the popup. The initial touch outside of the popup does not perform an action on the graphic element or screen.
Close
on the caption of the popup closes the popup. The initial touch outside of the popup does not perform an action on the graphic element or screen. Provide Feedback