Restore the default content of a predefined item

Restore the default content of a screen, popup, or
Banner
item in the
Predefined Screens
folder of the
Project Explorer
to overwrite any changes made to the item. For example, restore the content of the
Banner
item to have the default content appear at the top of screens.
To restore the default content of a predefined item
  1. With the revised item open, press
    CTRL+A
    to select all remaining content in the item and press
    Delete
    .
  2. Open another
    View Designer
    project and open the unchanged version of the item.
  3. With the unchanged item open, press
    CTRL+A
    to select all of the default content.
  4. Right-click a selected item and select
    Copy
    to copy the content to the clipboard.
  5. Right-click the empty revised item and select
    Paste
    . The default content of the item is restored.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal