Rename a popup

By default, the initial popup created in a project is named Popup_001. This number is incremented when creating new popups.
Rename a popup to make the name more meaningful. For example, give the popup a name that reflects the purpose, content, or targeted user of the popup. Names within a folder must be unique and are not case sensitive. For example, Bottling_Line and bottling_line are considered identical names. Renaming any popup in the
Predefined Screens
folder of the
Project Explorer
is not allowed.
To rename a popup
  1. In the
    Project Explorer
    , expand the
    User-Defined Screens
    folder.
  2. Double-click the popup to open the popup.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal