Remove the caption from a popup
Remove a caption from a popup so the caption no longer appears at the top of a popup. A popup cannot move on the HMI device if the popup does not have a caption.
To remove the caption from a popup
- In theProject Explorer, expand theUser-Defined Screensfolder.
- Select the popup.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- Clear theCaptionVisiblecheck box. The caption is removed from the popup.
Provide Feedback