Change the update rate of a screen, popup, or the System Banner

Screens, popups and the
System Banner
have a default update rate of 500 milliseconds. Use the
UpdateRate
property to change the frequency rate for an element.
TIP:
If the high update rate negatively impacts performance, the HMI device automatically lowers the update rate value.
To change the update rate of a screen, popup, or the System Banner
  1. In the
    Project Explorer
    , expand the
    User-Defined Screens
    or the
    Predefined Screens
    folder.
  2. Select the item to change.
  3. In the
    Properties
    window, select the
    Properties
    tab.
  4. Expand the
    General
    category.
  5. In
    UpdateRate
    , select the rate.
    • 100 ms
    • 250 ms
    • 500 ms
      TIP:
      Tips:
      • For best performance, on a
        PanelView
        5310 HMI device use:
        • Up to 600 tag references on a screen at 500 ms update rate
        • Up to 200 tag references on a screen at 250 ms update rate
        • Up to 100 tag references on a screen at 100 ms update rate
      • For best performance, on a
        PanelView
        5510 HMI device use:
        • Up to 800 tag references on a screen at 500 ms update rate
        • Up to 300 tag references on a screen at 250 ms update rate
        • Up to 150 tag references on a screen at 100 ms update rate
      • It is possible to use up to 2000 tag references on one screen, however, using more references than listed above may cause the HMI device to skip updates.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal