Change the opacity of a popup
Change the transparency level of a popup to make the popup more or less opaque. Make a popup less opaque to see graphic elements behind the popup when it opens on the HMI device.
To change the opacity of a popup
- In theProject Explorer, expand theUser-Defined Screensfolder.
- Select the popup.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- In theBackgroundOpacitybox, enter the opacity percentage:
- 0 (fully transparent) - 100 (fully opaque)
Provide Feedback