Change the background color of a popup

Change the background color of a popup to a different color, gradient color, or custom color. Radial gradients are not supported for popup fill color.
To change the background color of a popup
    1. In the
      Project Explorer
      , expand the
      User-Defined Screens
      folder.
    2. Double-click the popup to open the popup.
  1. In the
    Properties
    window, click the
    Properties
    tab.
  2. Expand the
    Appearance
    category.
  3. In the
    FillColor
    box, select a color using one of these methods:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal