Add popups to cache
Add popups to cache to decrease their loading time. The cache size is 20 MB and may not contain all of the popups in the project. Consider assigning only those popups that HMI operators open frequently. Popups upload to cache in the order they are placed in the
Predefined Screens
folder.To add popups to cache:
- In theProject Explorer, expand theUser-Defined Screensor thePredefined Screensfolder.
- Select a popup.
- In thePropertieswindow, select thePropertiestab.
- Expand theGeneralcategory.
- Select theCacheableproperty.
- Repeat for each popup you want to add to cache.
- SelectVerify Project.View Designerdisplays a warning message for each Cacheable property that did not fit into the cache.
Provide Feedback