Import Languages dialog box
How do I open the Import languages dialog box?
On the
Menu
bar, click Tools > Import Languages
.Use the
Import Languages
dialog box to add the languages to a View Designer
project. Add up to 20 different languages in one application.View Designer
creates and exports a language file that contains the user-editable text strings in a project. After the strings are translated, import the language file to add the languages to the project.Use the
Import Languages
dialog box to:- Select the translated language file.
- View the language changes made to theView Designerproject.
Provide Feedback