Add an event command to change the language on the HMI device
Create an event command to change that language that displays the runtime application on the HMI device.
Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs whenpressing the specified key.
- Key release.Occurs when releasing the specified key.
- Expand the Language category and select
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Switch Language. - In theSwitch Language Tolist, select a language.
Provide Feedback