Configure network-based security logon using Active Directory
Network-based security enables managing user accounts and user groups centrally. It allows
network users to log on to an HMI device, authenticate with the Active Directory, and be
granted authorization rights based on their role.
When network-based logon is used for a project, local users still may be configured and used
on the terminal (for example for back-up). You can switch to local users on the logon pop-up
in runtime.
Active Directory properties may vary depending on your company and the complexity of system
architecture. If you find any problems during configuration, contact your Active Directory
administrator.
TIP:
Leaving the
Connection
fields
blank will have the panel use local users at runtime.Ensure that the logon method is set to use the user name and password:
- From the main menu, selectProject> Project Properties.
- In theProject Propertieswindow, select theLog On Methodtab.
- Select theUse user name/password for logging onradio button.
To configure network-based security logon:
- From the main menu, selectTools->Security Administration.
- In the Security Administration window, select theConnection and Groupstab.
- In theConnectionsection, fill in the required fields.
- In theDomain Namefield, enter your corporate domain.IMPORTANT:During the Active Directory logon process,user nameand configuredDomain nameare combined to define theUser Principal Name,in the format <username>@<domain>.com. It is sent with a password to the domain controller for authentication.The username used for theUser Principal Namemust be used during Active Directory logon.Correct format: jamessmith@domain.com,Incorrect format: domain.com\jsmith
- In theDomain Controllerfield, enter the full address of the Active Directory server.
- In thePortfield, enter the number of the port.TIP: Typical default ports are: no encryption – 389, StartTLS – 389, LDAPS – 636.
- In theDomain Distinguished Namefield, enter your domain distinguished name.DC=domain,DC=com
- If the connection requires encryption, select the encryption method.IMPORTANT: Not using encryption for network-based authentication results in sending username and password as plain text over the network. This creates a security risk.To use StartTLS or LDAPS encryption for logon, you are required to import the proper security certificate to the terminal by using the Certificates setting screen.
- In the Groups and Roles section, click
next to Add new User Group.TIP: You can add and define multiple groups. - In the new section that appears, enter the following information:
- In theUser Group Distinguished Namefield, enter a distinguished name of a group.CN=Operators,OU=Groups,DC=domain,DC=com
- In the drop-down menu next to theUser Group Distinguished Namefield, select the role you want to assign to the group.At runtime, when someone logs in, the Active Directory returns the group membership of that user. Now this group is mapped to a role, so the user gets the security role mapped to the Active Directory group they belong to. If a user belongs to multiple groups with different roles, they will get the first role configured in this list. If a user does not belong to any group mappings, the user will receive an error message on the PanelView 5000 when they log on.TIP: You can remove a group by clicking
.
- ClickOK.TIP: Active Directory properties may vary, depending on your company and complexity of the system architecture. If You encounter any problems during configuration, contact your Active Directory administrator to obtain guidance or this configuration.
See also
Provide Feedback