Delete a graphic element from the definition of an Add-On Graphic

Delete a graphic element from the definition of an Add-On Graphic to change the appearance of the Add-On Graphic. The graphic element is removed from every instance of the Add-On Graphic in the project.
Deleting graphic elements may change the size of the Add-On Graphic. The size of Add-On Graphic instances is not affected by deleting a graphic element from the definition. Instances of the Add-On Graphic are scaled to fit the content changed in the definition of the Add-On Graphic.
To delete a graphic element from the definition of an Add-On Graphic
  1. In the Project Explorer, expand the
    Assets
    and
    Add-On Graphics
    folders.
  2. Double-click the Add-On Graphic. The definition of the Add-On Graphic opens in a separate tab.
  1. TIP:
    Tips:
    • Right-click the Add-On Graphic and select
      Open
      or press
      Enter
      when the Add-On Graphic is selected to open the definition.
    • If an instance of the Add-On Graphic exists on a screen, right-click the Add-On Graphic on the screen or in the
      Graphic Explorer
      and then select
      Open Graphic Definition
      to open the definition. The
      Open Graphic Definition
      option is unavailable for selected groups and multiple selected graphic elements, even if the selection contains an Add-On Graphic.
    Select the graphic element to delete and press
    Delete
    .
    TIP:
    Deleting the graphic element that is closest to the boundary of the Add-On Graphic causes the background of the Add-On Graphic to resize to fit the remaining graphic elements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal