Side navigation menu contents
Folders and shortcuts in the
Navigation Menu
folder of the Project Explorer to which you are granted security access appear in the Navigation Menu
on the HMI device.The side navigation menu shows up to four levels of nesting.

Item | Description |
![]() | Finds the strings in the whole Navigation menu , regardless of the level of nesting and highlights it yellow. |
![]() | The navigation menu contains the Home screen for the project and folders and shortcuts placed at the root level of the Navigation Menu folder in the Project Explorer . By default, the main menu includes Alarm Summary , Alarm Manager , Alarm History , Automatic Diagnostics , Auto Dial History , and Settings items. These items appear in the Predefined Screens folder of the Project Explorer. These items open tables to view and manage alarms, and a screen to configure settings for the HMI device. |
TIP:
You can use your keyboard to navigate through the menu:
- Tab - activates the menu keyboard navigation.
- Arrows - enable moving up and down through the menu.
- Enter - opens the screen, selected from the menu.
After opening a selected screen, the navigation menu item is marked blue.
Provide Feedback