Emulate Project dialog box

The
Emulate Project
dialog box indicates that
View Designer
:
  • Downloads the project to the Emulator
  • Builds the runtime application
  • Starts the runtime application
    The
    Emulate Project
    dialog box closes automatically when the application starts and the
    View 5000 Emulator
    window opens to depict the project.
TIP:
Tips:
  • The verification process when downloading a project to the Emulator is the same verification process that occurs when downloading a project to the HMI device. The process verifies the syntax of all expressions, the elements and properties referenced in expressions, and the existence of all project tags in the referenced controller projects.
  • If
    View Designer
    encounters a problem, the
    Emulate Project
    window indicates that there is an error. Any errors to correct appear in the
    Errors
    window below the
    View Designer
    screen. Select
    Close
    to close the
    Emulate Project
    window, use the
    Errors
    window to navigate to the source of the error. Resolve all errors before restarting the Emulator.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal