Start the Emulator
Start the Emulator to view and test the behavior of the open project. This verifies the project before downloading it to the Emulator. Emulate a project for each open instance of
View Designer
.Prerequisites
- Add controller references to the project and set theEmulator to Controller pathin theReferencestab for each referenced controller in the project properties. This path allows the Emulator to emulate the data from theLogix Designerproject file (.acd) in theView Designerproject file (.vpd).TIP:Setting the Emulator to Controller path to the same path for multiple controller references displays duplicate alarms in the Alarm Summary and the Alarm Manager. Each alarm in the controller displays for each controller reference that has the same Emulator to Controller path.
- To emulate a different project, close theView 5000 Emulatorwindow. Only one instance of the Emulator can run on a computer at one time.
To start the Emulator
- In the open project, select
Emulate Project. TheEmulate Projectdialog opens and shows progress asView Designerverifies and then starts the runtime application. TheEmulate Projectdialog box closes automatically when the Emulator starts. - TheTIP:Tips:
- The verification process when downloading a project to the Emulator is the same verification process that occurs when downloading a project to the HMI device. The process verifies the syntax of all expressions, the elements and properties referenced in expressions, and the existence of all project tags in the referenced controller projects.
- IfView Designerencounters a problem, theEmulate Projectwindow indicates that there is an error. Any errors to correct appear in theErrorswindow below theView Designerscreen. SelectCloseto close theEmulate Projectwindow, use theErrorswindow to navigate to the source of the error. Resolve all errors before restarting the Emulator.
View 5000 Emulatorwindow opens and shows the initial screen of the project and the specifiedPanelView5000 HMI device. - Interact with the project in theView 5000 Emulatorwindow:
- Interact with screens in the project as if the screen appears on the targetPanelView5000 HMI device. For example, select items.
- Interact with the HMI device by selecting buttons on the depictedPanelView5000 HMI device.
- Interact with the HMI device through an external keyboard:
- L1throughL10on an HMI device keypad correspond withShift+F1throughShift+F10on an external keyboard.
- R1throughR10on an HMI device keypad correspond withCtrl+F1throughCtrl+F10on an external keyboard.TIP:Tips:
- SelectingPROJECT > Emulate Projectstarts the Emulator.
- View Designerdoes not emulate changes made to the project after the starting the Emulator. Close and restart the Emulator to continue emulating the project.
- The Emulator does not support:
- HMIBC buttons.
- Certain settings and interactions with the HMI device:
- Rebooting the HMI device.
- Calibrating the touch screen of an HMI device.
- Changing the brightness of the HMI device.
- Changing the IP address of the HMI device.
- Viewing diagnostic information for the HMI device.
- Configuring the date and time of the HMI device.
- Setting the time zone of the HMI device.
- Configuring the screen saver of the HMI device.
- Importing a troubleshooting profile.
- Exporting a troubleshooting log.
Provide Feedback