Details pane for Automatic Diagnostics History
Select
on an automatic diagnostics history table to open the
Details
on an automatic diagnostics history table to open the Details
pane.In a medium Automatic Diagnostics History table intended for HMI devices with seven-inch to nine-inch screens, the
Details
pane replaces the list of automatic diagnostics in the table. In a large Automatic Diagnostics History table intended for HMI devices with ten-inch or larger screens, the Details
pane opens at bottom of the automatic diagnostics table.
Item | Description |
|---|---|
![]() | The Details pane with additional details for the selected automatic diagnostics history. This pane displays data, such as Message, Event Time, Diagnostic Code and State Change. When multiple diagnostics are selected, details display for the last selected automatic diagnostics. |
![]() | Buttons to perform operations on diagnostics in the |
The contents of the
Details
pane appears in rows.Row | Description |
|---|---|
Message | The message with a fault description. |
Device Name | The name of a controller for which the automatic diagnostics occurred for. |
Product Name | The Rockwell Automation product for which the diagnostics occurred for. |
Event Time | The date and time the automatic diagnostics event occurred. |
State | The state of an automatic diagnostics. |
State Change | The last state change performed on the diagnostics. |
Diagnostics Code | The type of diagnostics that occurred. |
Resource | The resource that reports a fault. |
Catalog | The device catalog number. |
Product Type | The detailed information about the device that reports the fault. |
Vendor | The vendor of the reporting device. |
Version | The firmware version of the reporting device. |
Provide Feedback