Automatic Diagnostics History contents for a medium HMI device screen
The
Automatic Diagnostics History Viewer Medium
table appears on the predefined Automatic Diagnostics History
screen. This screen is in the Predefined Screens
folder of the Project Explorer
. The table is recommended for six- to nine-inch HMI device screens. Create an Automatic Diagnostics History Medium
table with customized appearance and content or change the Automatic Diagnostics History Medium
table on the predefined Automatic Diagnostics History
screen. 
Item | Description | |
|---|---|---|
![]() | The list of automatic diagnostics state changes records from the terminal. | |
![]() | Buttons to perform actions available for the Automatic Diagnostics History Viewer: | |
![]() | Details hides or shows the Details pane, which contains the details of the last selected automatic diagnostics state change record. The Details pane replaces the list of diagnostics in medium automatic diagnostics tables. If no record is selected, the Details pane is empty. | |
![]() | Refresh loads the latest diagnostics state changes from the automatic diagnostics history. The operator has to refresh the table to see the latest changes. To display the latest state changes, close and reopen the Automatic Diagnostics History viewer. | |
![]() | Help opens the Help popup. This popup displays a legend of icons and the task each button on an automatic diagnostics history table performs. | |
Provide Feedback