Automatic Diagnostics History contents for a large HMI device screen
The
Automatic Diagnostics History Viewer Large
table appears on the predefined Automatic Diagnostics History
screen. This screen is in the Predefined Screens
folder of the Project Explorer
. The table exists for ten-inch or larger HMI device screens. Create an Automatic Diagnostics History Large
table with customized appearance and content or change the Automatic Diagnostics History Large
table on the predefined Automatic Diagnostics History
screen. 
Item | Description | |
|---|---|---|
![]() | The list of automatic diagnostics state changes records from the terminal. | |
![]() | Buttons to perform actions available on the Automatic Diagnostics History table: | |
![]() | Details hides or shows the Details pane, which contains the details of the last selected automatic diagnostics state change record. The Details pane appears on the bottom half of large automatic diagnostics history tables. If no record is selected, the Details pane is empty. | |
![]() | Refresh loads the latest diagnostics state changes from the automatic diagnostics history. The operator has to refresh the table to see the latest changes. To display the latest state changes, close and reopen the Automatic Diagnostics History viewer. | |
![]() | Help opens the Help popup. This popup displays a legend of icons and the task each button on an automatic diagnostics table performs. | |
Provide Feedback