Specify the visibility of an alarm table

Specify if an alarm table is always visible on the HMI device screen. Bind the visibility of an alarm table to a tag value to display the alarm table only when the specified tag value is true. For example, bind visibility to a tag to indicate there is a problem in the system. If binding the alarm table to a tag value, the table appears on the HMI device screen only when the tag is true.
To specify the visibility of an alarm table
  1. On the screen, select the alarm table.
  1. In the
    Properties
    window, click the
    Properties
    tab.
  2. Expand the
    Appearance
    category.
  3. In the
    Visible
    box, select an option:
    • Visible
      (selected)
    • Not visible
      (cleared)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal