Specify the default sort order of alarm table contents
Determine how alarm table content is initially sorted on the HMI device screen. Specify which columns to sort and in which order, and whether to sort the contents of a column in ascending or descending order.
To specify the default sort order of alarm table contents
- On the screen, select the alarm table.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory. In theSortOrderbox, enter columns and their order:
- A valid column number, colon, and a D for descending or A for ascending. For example, 1:D,2:D provides a primary sort of Column 1 in descending order, and a secondary sort of Column 2 in descending order. You can enter a value for each column in the table.
Provide Feedback