Configure alarm table rows for readability and touch
Configure properties to affect the displayed font, font size, and row padding (the distance between cell contents and cell borders) in a table. Font size affects row height. Padding is required to make tapping rows feasible on an HMI device. Using a small font size and no padding makes it difficult to tap a single row in an alarm table on the HMI device. Row height is determined by the
FontSize
property value and twice the value of the RowPadding
property. The default combined FontSize
(nine points) and RowPadding
(14 pixels) property values result in an approximate row height of one-third inch. There is no minimum or maximum font size or row padding. To be able to tap single alarm rows on the HMI device, specify reasonable font sizes and row padding for a table.To configure alarm table rows for readability and touch
- On the screen, select the alarm table.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancenode.
- To make sure the alarm table is readable and allows enough room within rows for touch, configure the properties:
- FontName.Select a font.
- FontSize. Enter a font size readable for users on the HMI device.
- RowPadding.Enter the distance, in pixels, between cell content and the cell border.The selectedFontName,FontSize, andRowPaddingproperty values are reflected in the sample data of the alarm table. The changes are also reflected in the alarm table on the HMI device. Changes to these properties are not reflected in theDetailspane of an alarm table.
Provide Feedback