Change the opacity of an alarm table

Change the opacity level of an alarm table to make it more or less transparent.
To change the opacity of an alarm table
  1. On the screen, select the alarm table.
  1. In the
    Properties
    window, click the
    Properties
    tab.
  2. Expand the
    Appearance
    category.
  3. In the
    Opacity
    box, enter a percentage. 0 is fully transparent and 100 is fully opaque.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal