Create an Alarm History table
Add an Alarm History graphic element to a screen to create a screen on the HMI device to view the history of alarm state changes.
Prerequisites
- Configure ALMA and ALMD alarm instructions inLogix Designeror add tag-based alarms in aLogix Designer. The 5380, 5480 and 5580 Logix families of controllers support tag-based alarms.
To create an Alarm History screen
- In theAlarmscategory of theToolbox, double-click or drag and drop theAlarm History Largeor theAlarm History Mediumgraphic element onto the screen.
Provide Feedback