Change the width of a column in an Alarm History table
Change the width of a column in an Alarm History table if the data in the column is wider than the current width of the column. Use the sample data in a column to determine the required column width. The sample data represents the length of data anticipated for a column.
To change the width of a column in an Alarm History table
- On the screen, select Alarm History.
- In thePropertieswindow, select theColumnstab.
- In the
- In the column card, clickShow/Hide
to expand the column card. The selected column card is outlined in blue.
Widthfield at the bottom of the column card, enter a positive number for the column width, in pixels.Changes to column width are saved automatically. The last column added fills the remaining space in the row. If the total width of all columns exceeds the width of the table, a horizontal scroll bar appears at the bottom of the table.TIP:When resizing a column in an Alarm History table, leave some space between the text of the column heading and the border of the column. If the text of a column heading appears at the column border, the text of the column heading may appear clipped in theAlarm Historyon the HMI device
Provide Feedback