Change the order of columns in Alarm History table
The columns in the table on the predefined
Alarm History
screen appear in a default order. This screen is in the Predefined Screens
folder of the Project Explorer
. To change the order of columns in an Alarm History table
- On the screen, selectAlarm History.
- In thePropertieswindow, select theColumnstab.
- Point to the column card heading and clickMove column up
move the column to the left or Move column down
to move the column to the right. Reordered columns appear in the Alarm History table on the screen.
Provide Feedback