Alarm History contents for a large HMI device screen
The
Alarm History Large
alarm table appears on the predefined Alarm History
screen. This screen is in the Predefined Screens
folder of the Project Explorer
. The table is recommended for large, ten-inch or larger HMI device screens.
Item | Description | |
|---|---|---|
![]() | The list of alarm state changes records from the alarm log. | |
![]() | Buttons to perform operations on alarms in the Alarm History table: | |
![]() | Details hides or shows the Details pane, which contains the details of the last selected alarm. The Details pane appears on the bottom half of large alarm tables and replaces the list of alarms in medium alarm tables. If no alarm is selected, the Details pane is empty. | |
![]() | Refresh loads the latest alarm state changes from the alarm history. You can also exit and enter the screen with the Alarm History again to refresh with the latest changes. | |
![]() | Help opens the Help popup. This popup displays a legend of icons for In Alarm/Unacknowledged, Normal/Unacknowledged, In Alarm/Acknowledged, and Faulted alarms, and the task each button on an alarm table performs. | |
![]() | Filter list. Select a filter in the HMI device to list only the alarm state change records containing the filter value for the indicated column. For example, if the filter exists, select the filter Priority:High to show only those alarm state changes with a high priority. Configure filters in View Designer . | |
Provide Feedback