Add a column to Alarm History Viewer

New columns in an
Alarm History
appear on the right side of the table with sample data in each column. Use the sample data to determine the column width of a column.
To add a column to an Alarm History table
  1. On the screen, select the
    Alarm History
    .
  2. In the
    Properties
    window, select the
    Columns
    tab.
  3. Select
    Add Column
    .
  4. Select the data to display in the column. The selected column appears in the heading of the new card.
  5. Change the width of a column to display the data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal