New Project dialog box
How do I open the New Project dialog box?
On the
Menu
bar, click File > New Project.
Use the
View
tab on the New Project
dialog box to:- Create and name aView Designerproject.AView Designerproject includes the screens that you create, controller references, and information about the target HMI device. The project is stored in a file with a .vpd extension.
- Select the type of HMI device.The screens in a project represent the physical size of the HMI device selected for the project.
- Optionally, select theView Designerversion with which to create the project when there are multiple versions ofView Designerinstalled.
Creating a project is the first step in building a runtime application.
Tip: | Close any open project before creating another project. Projects in other instances of View Designer may remain open. It is recommended that no more than three instances of View Designer run at one time. |
Provide Feedback