Errors window
How do I open the Errors window?
The
Errors
window opens automatically to display the invalid tags or expressions detected during project verification.To open the
Errors
window manually, on the Menu
bar, click View > Errors
.The
Errors
window displays the results of project verification. It opens when View Designer
detects invalid tags or expressions. Downloading a project automatically verifies that project. Verify a project at any time during project development. For example, verify a project if a controller is defined for the project. Project verification verifies:
- The syntax of all expressions contained in theView Designerproject
- The validity of parameters passed from one item to another and required error messages
- The existence of elements and properties referenced in an expression
- The existence of tags in theView Designerproject in the referenced controller projects
- That Add-On Graphics do not contain direct bindings to controller tags or system tags
- That property bindings in the definition of an Add-On Graphic are formatted as ElementName.PropertyName
- That aliased properties of graphic elements in the definition of an Add-On Graphic are not bound
- That all tags in the data logs are valid.
Errors
window to:- View the errors and warnings detected during project verification.
- Navigate to the source of the error or warning so that you can resolve the problem.
- Sort the results to group them by severity level, description, or location in the project.
Provide Feedback