Verify Project dialog box
How do I open the Verify Project dialog box?
On the
Menu
bar, click Project > Verify Project
.The
Verify Project
dialog box displays the progress of the project verification process. Project verification verifies:
- The syntax of all expressions contained in theView Designerproject
- The validity of parameters passed from one item to another and required error messages
- The existence of elements and properties referenced in an expression
- The existence of tags in theView Designerproject in the referenced controller projects
- That Add-On Graphics do not contain direct bindings to controller tags or system tags
- That property bindings in the definition of an Add-On Graphic are formatted as ElementName.PropertyName
- That aliased properties of graphic elements in the definition of an Add-On Graphic are not bound
- That all tags in the data logs are valid.
Errors
window displays the invalid tags and expressions detected by the project verification process. Provide Feedback