Define conventions for screens

To increase application usability and operator efficiency, follow established conventions and good visual design principles when creating screens.
Prerequisites
Decide the specific settings to use for items before creating screens:
  • Colors, background colors, and fonts
  • Equipment symbols
  • Position and status of valves
  • Position and status of pumps and motors
  • Information to be included on each screen such as a company logo.
Consistency considerations
Follow guidelines to make the screens within the application consistent:
  • Present the same information and basic functions in the same places on each display to make it easier for users to find elements as they navigate from screen to screen.
  • Use the standard and easily recognizable symbols from the
    View Designer
    library of predefined graphics. For example,
    View Designer
    contains standard ISA symbols for tanks and valves.
  • Place the same kind of buttons in the same positions on each screen, and label them consistently. For example, if there is a Start button in a certain position in one screen, do not put a Stop button in the same position on another screen.
  • Use standard, clear terminology. Avoid abbreviations or acronyms.
  • Use colors with recognizable meanings. For example, in Europe and North America, the colors red and green often mean stop and start. Keep color meanings consistent by assigning red only to Stop buttons, and green only to Start buttons.
Usability considerations
Follow guidelines to increase application usability:
  • On each screen, include only necessary information. Create pop-ups to provide more detailed information.
  • For touch screens, place important buttons where they will not be blocked by a pop-up. Also ensure that buttons are large enough and spaced far enough apart for users to touch them easily, even when they are wearing work gloves.
  • Ensure there is always a clear way to move between displays.
  • For text, use high-contrast color combinations such as yellow on blue or dark text on light-colored backgrounds.
Reuse considerations
After establishing conventions for screens, ensure screen uniformity by reusing screens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal