State Table Definition dialog box

How do I open the State Table Definition dialog box?
On the
Properties
window, click the
Animations
tab. Click
Add Animation
and click
State Table.
Use the
State Table
to configure animations to affect the Appearance, Position and Size, or General properties (for example, visibility, rotation angle, fill color) of a graphic element, Add-On Graphic, or screen. To use a State Enter or a State Exit event to drive animation, create a
State Table
before creating the event.
Configure multiple states for each graphic element and Add-On Graphic. Configure more than one
State Table
per graphic element and Add-On Graphic.
Use the
State Table Definition
dialog box to:
  • Specify the number of states to animate.
  • Select the properties to animate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal