Animations tab

How do I open the Animations tab?
On the
Properties
window, click the
Animations
tab.
Use animation to enhance the graphical representation of the state of a machine or process on the HMI device. This can mean hiding or showing graphic elements, including Add-On Graphics, and changing the appearance of the elements or moving them on the screen.
Use the
Animations
tab to:
  • Use a
    Color Table
    or a
    State Table
    to animate a graphic element or screen.
  • Add or delete an animation.
  • Configure or change an animation.
  • View the animations associated with a graphic element or screen.
Use a
Color Table
to:
  • Affect only the color properties of a graphic element or screen (for example, fill color, button color, border color).
Use a
State Table
to:
  • Affect the Appearance, Position and Size, or General properties (for example, height, width, rotation angle) for a graphic element or screen.
  • Use a State Enter or State Exit event to trigger a command (for example, write a tag value to a controller when the
    State Table
    enters a specific state).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal