Color Table Definition dialog box
How do I open the Color Table Definition dialog box?
On the
Properties
window, click the Animations
tab. Click Add Animation
and click Color Table.
Use a
Color Table
to configure animations that can affect any or all of the color properties (for example, fill color, color, font color) of a graphic element, Add-On Graphic, or screen. Configure multiple color states and multiple
Color Tables
for a graphic element or Add-On Graphic.Use the
Color Table Definition
dialog box to:- Specify the number of states.
- Select the properties to animate.
Provide Feedback