Rename a PDF document
Renaming a PDF document in the
Documents
folder renames every instance of the PDF document in the project. The name of the PDF document changes in each instance of a PDF graphic element and PDF Viewer Add-On Graphic in the project. To rename a PDF
- In theAssetsfolder in theProject Explorer, locate the PDF document in theDocumentsfolder.
- Click the PDF document once to select the item.
- Click the PDF document again and type the new name.TIP:Tips:
- Right-clicking the name of the PDF, clickingRename, and entering a new name also renames the PDF.
- The name must contain only numbers, letters, and underscores.
- The name must not begin with a number, contain spaces, have more than one underscore in a row, or end with an underscore.
- Renaming an existing PDF document applies the new name to all PDF graphic elements and PDF Viewer Add-On Graphics that reference the PDF document.
IMPORTANT:
Renaming a PDF document in the
Documents
folder does not change the file name of the PDF document. Expand the folder and select the PDF document. Expand the General
category in the Properties
window to see the name of the PDF document.Provide Feedback