Delete a PDF document from a project
Deleting a PDF from the
Documents
folder: - Removes the PDF document from all screens, popups, and Add-On Graphics in the project that reference the PDF.
- Deletes the references to the PDF from instances of PDF graphic elements and PDF Viewer Add-On Graphics in the project.
- Removes the name from theDocumentNameproperty in thePropertiestab for each PDF graphic element and PDF Viewer Add-On Graphic in the project.
The screen containing the PDF graphic element and PDF Viewer Add-On Graphic displays a red outline and a message to select a PDF document when there is no referenced PDF.
IMPORTANT:
Deleting a PDF document cannot be undone. Re-adding a deleted PDF document to a project does not restore the configuration of the PDF document in instances of the PDF graphic element or PDF Viewer Add-On Graphic in the project.
To delete a PDF document from a project
- In theProject Explorer, open theAssets > Documentsfolder.
- Right-click the PDF document and selectDelete. A prompt appears if a PDF graphic element or PDF Viewer Add-On Graphic in the project references the PDF document.
- SelectYesto delete the PDF document orNoto not delete the PDF document from the project.
Provide Feedback