Work with individual graphic elements or groups in a group
You can change the appearance, position, and size of individual graphic elements or groups in a group. You can bind to the individual properties and attach events or animations.
To work with individual graphic elements or groups in a group:
- In the Graphic Explorer, expand the group and select the graphic element.
- To select multiple graphic elements, press and hold Ctrl while you click each graphic element.
- Use the tabs on the Properties window to change the properties and create animations and events for the selected graphic element.
Tip:You can also edit the size and angle of individual elements or groups on the screen:- Double-click any element in a group to put the group in the editing mode.
- Select the element you want to edit.
- Use the arrows to change the size, angle, and position of the element or group.
Tip:You can change the position of elements or groups by selecting, dragging and dropping them in the Graphic Explorer.
Tip: Multiselect is only possible for the elements on the same level of nesting.
Provide Feedback