Ungroup graphic elements
Ungroup graphic elements and Add-On Graphics when you no longer need to work with multiple elements as a group.
IMPORTANT:
You cannot undo an Ungroup operation.
When ungrouping, animations and events configured for the group, as well as the bindings to properties of the group, are lost. Bindings and expressions that reference graphic elements and Add-On Graphics that are part of the group still function.
To ungroup graphic elements:
- On the screen, right-click the group and selectUngroup.
- If you ungroup a rotated group, the Angle value is applied to the graphic elements within the group.
Provide Feedback