Flip a group or an element in a group
Flip a group or an element in a group to create a reverse image of it. Graphic elements in a group that contain text do not flip.
The Angle property displays the new rotation angle. The new angle is calculated using the following equation: NewAngle = 360 - OldAngle. For example, a group with an Angle value of 45 (45 degrees) before being flipped displays an Angle value of 315 (315 degrees) after being flipped.
To flip a group:
- On the screen or in theGraphic Explorer, right-click the group or a graphic element and clickFlip.
- Select one of the options:
- Horizontal. Flips the group along its horizontal axis.
- Vertical. Flips the group along its vertical axis.TIP:Alternate methods to flip a group:
- On theDrawingtoolbar, click theFlipdown arrow, and select an option.
- On theMenubar, clickArrange > Flip, and select an option.
Provide Feedback