Duplicate a group
Use the
Duplicate
command to make a copy of a group. Duplicating a group duplicates the property values, animations, and events associated with the group.
IMPORTANT:
Duplicating a group of graphic elements that reference properties of those graphic elements breaks the property references in the duplicated groups. This is because duplicating a group increments the name of the elements contained in the group. The reference remains unchanged. Due o the incremented names, update the bindings and expressions that reference the elements within the new group. Changes to graphic element names do not propagate automatically.
To duplicate a group:
- Select the group and pressCtrl+D.TIP:Tips:
- Continue to create copies until de-selecting the group.
- Duplicated contents are not placed in the clipboard.
Provide Feedback