Cut, copy, paste, or delete a group or an element in a group
Cut, copy, and paste a group on a single screen, across multiple screens, and between projects.
Important: | Copying and pasting a group of graphic elements that reference properties of those graphic elements will break the property references in the copied groups. This is because copying and pasting a graphic element increments the name of the element, including elements contained in a group. However, the reference remains unchanged. If you update bindings and expressions that reference the name of the graphic element, changes to graphic element names are not propagated automatically. |
TIP:
You can paste graphic elements stored in the clipboard to an edited group directly on the screen or in the Graphic Explorer by selecting any element in the target group destination.
To cut, copy, paste or delete a group or an element in a group
- Right-click an item on the screen or in the Graphic Explorer and select the option:
- Cut.From the context menu, selectCut.TIP:Alternate methods for cutting:
- On the keyboard, pressCtrl+X
- On theMenubar, clickEDIT > Cut.
On theStandardtoolbar, clickCut
- On the keyboard, pressCtrl+X
- On theMenubar, clickEDIT > Cut.
On theStandardtoolbar, clickCut
. Alternate methods for cutting:- On the keyboard, pressCtrl+X
- On theMenubar, selectEDIT > Cut
- On theStandardtoolbar, selectCut
.
- Copy.From the context menu, selectCopy.TIP:Alternate methods for copying:
- On the keyboard, pressCtrl+C
- On theMenubar, selectEDIT > Copy
- On theStandardtoolbar, clickCopy
.
- Paste.From the context menu, selectPaste.TIP:Alternate methods for pasting:
- On the keyboard, pressCtrl+V
- On theMenubar, clickEDIT > Paste.
On theStandardtoolbar, clickPaste
- On the keyboard, pressCtrl+V
- On theMenubar, clickEDIT > Paste.
On theStandardtoolbar, clickPaste
- On the keyboard, pressCtrl+V
- On theMenubar, clickEDIT > Paste.
On theStandardtoolbar, clickPaste
. Alternate methods for pasting:- On the keyboard, pressCtrl+V
- On theMenubar, clickEDIT > Paste.
On theStandardtoolbar, clickPaste
. Alternate methods for pasting:- On the keyboard, pressCtrl+V
- On theMenubar, clickEDIT > Paste
- On theStandardtoolbar, clickPaste
.
- Delete.From the context menu, selectDelete.TIP:Alternate methods for deleting:
- On the keyboard, pressCtrl+X
- On theMenubar, clickEDIT > Delete.
Provide Feedback