Add a graphic element or a group to a group
Add graphic elements or groups to a group.
To add a graphic element or group to a group on the screen:
- Add an element or group to the screen.
- Copy or cut the element.
- Double-click any element in a target group to put the group in the editing mode.
- Paste the new element or group.IMPORTANT:Clicking anywhere on the canvas when the group is in the editing mode unselects the group.
To add a graphic element or group to a group in Graphic Explorer:
- Add an element or group to the screen. It automatically appears in the Graphic Explorer.
- Select an element or elements you want to add to a group.
- Drag and drop the element or elements in the desired group.
Provide Feedback