List of displays is empty or missing displays
After you select a FactoryTalk View application, if the list of graphic displays is empty or does not contain all of the displays you expect to see, consider the following potential causes and remedies.
Incorrect
FactoryTalk View
applicationThe displays you are looking for may not be contained in the
FactoryTalk View
application you selected.- Verify you selected your intendedFactoryTalk Viewapplication.
Incorrect Application Type
The displays you are looking for may be in an application located in another
FactoryTalk Directory
.- From the navigation bar, selectPublish Displays.
- From theSelect alist, select an application type.FactoryTalk Viewapplication type
- Site Edition (Network Distributed)- shows applications from theFactoryTalkNetwork Directory specified in the.FactoryTalk DirectoryServer Location Utility
- Site Edition (Network Station)- shows applications from theFactoryTalkNetwork Directory on the computer that hosts theFactoryTalk ViewPointserver.
- Site Edition (Local)- shows applications from theFactoryTalkLocal Directory on the computer that hosts theFactoryTalk ViewPointserver.
FactoryTalk ViewPoint Administration
requires refreshIf you are modifying or creating new displays in
FactoryTalk View
while FactoryTalk ViewPoint Administration
is open, the list of screens will not be updated until the web page is refreshed.- PressF5to refreshFactoryTalk ViewPoint Administrationwith any new application content.FactoryTalk ViewPoint Administrationshows the Home page.
- ClickPublish Displays.
- Select theFactoryTalk Viewapplication you are working on and then click2 Select displays.The list of displays should now include any new displays you created inFactoryTalk View Studio.
Provide Feedback