Select a FactoryTalk View application

Select a
FactoryTalk View
application to publish one or more of its displays to
FactoryTalk ViewPoint
.
To select a
FactoryTalk View
application
  1. Click
    Start > All Programs > Rockwell Software >
    FactoryTalk ViewPoint
    , and then click
    FactoryTalk ViewPoint Administration
    .
  2. From the navigation bar, select
    Publish Displays
    .
  3. From the
    Select a
    FactoryTalk View
    application type
    list, select an application type.
    • Site Edition (Network Distributed)
      - shows applications from the
      FactoryTalk
      Network Directory specified in the
      FactoryTalk Directory
      Server Location Utility
      .
    • Site Edition (Network Station)
      - shows applications from the
      FactoryTalk
      Network Directory on the computer that hosts the
      FactoryTalk ViewPoint
      server.
    • Site Edition (Local)
      - shows applications from the
      FactoryTalk
      Local Directory on the computer that hosts the
      FactoryTalk ViewPoint
      server.
      TIP:
      • If you select Site Edition (Network Distributed) or (Network Station) but the
        FactoryTalk
        Network Directory does not contain any applications, verify the
        FactoryTalk Directory
        location is set correctly.
      • If you select Site Edition (Local) but the
        FactoryTalk
        Local Directory does not contain any applications, verify the application is hosted on the local machine.
  4. From the
    Select the application
    list, select a
    FactoryTalk View
    application to publish.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal