Change administration permissions
Once enabled, only users that belong to a
FactoryTalk Directory
group that has been granted administration permissions for FactoryTalk ViewPoint Administration
can manage FactoryTalk ViewPoint Administration
settings and publish graphic displays.Prerequisites
To change administration permissions
- Sign in towith an account that has administration permissions.FactoryTalk ViewPoint Administration
- From the navigation bar, clickSecurity Settings.
- (optional) If it is not selected, click theAdministrationtab.
- In theUser Groupstable, select or clear checkboxes to change administration permissions:
- Selected- User group has administration permissions
- Cleared- User group does not have administration permissions
- ClickApply.
Provide Feedback