Logon setup options
The following table shows the options on the
Logon
tab in the DeskLock Setup
dialog box.Options | Descriptions |
|---|---|
Automatically Logon to Windows | Select this box to go through the Windows logon procedure automatically, using the domain and user names and password specified. The user name and password are case sensitive. The password specified here for automatic logon is for Windows logon only. To set up a password for DeskLock, use the Password tab. |
Default Domain Name | This is the name of the domain you logged in with. |
Default User Name | This is the user name you logged in with. The user must have been created in the Windows User Manager and have administrator rights. If this user does not have administrative rights, there will be no way to reset operating system functionality. |
Default Password | Type the password to be used for automatic Windows logon. |
Confirm Password | Retype the password here to confirm it. |
Go to the background when it starts | Some users may see the DeskLock dialog box appear in front of the application(s) listed in the Programs section of the Desktop tab. Select this check box to ensure that the DeskLock dialog box is not visible at runtime. |
Provide Feedback